I'm using a TPS71701 in a 2.5V Supply.
The device is configured for 2.5V as described in the Datasheet, and the load current ist very low. I'm using a 10µF X5R Capacitor at the input and at the output. The input Voltage is 3.3V and the enble pin is connected to Vin.
Actually I have the following behavior:
At an Ambient Temperature of 30°C or less everything works fin, and the temperature of the device never goes higher than 65°C. But if I schwicht of the device after a certain time of operation, everything is roughly warmed up 50°C, then the starup of the device fails, and the output remains at 0V. If the temperature goes down to 20°C, the cycling of the supply is followed by normal operation. I can reconform the chip behavior also, if I warm up the unconnected device to 50°C, in thaat case I won't stat either.
I have this behavier in 10 out of thousand units, and the problem moves with the TPS71701 to an other unit.
Has anyone a tip for me?
Thanks,
Gerald