I want to use 80% of battery capacity as 100%.
In that case, what parameter should be changed?
Is it the following parameters? If there are any others, please tell me.
-Charge voltage: setting lower voltage than 4.2V
-Design Capacity: setting lower value than capacity of cell datasheet
-Qmax: same as above "Design Capacity"
Even if there is the GG file after 4.2V learning cycle, should the learning cycle be done again at lower setting?