Is there a reason why I need to keep the inductor ripple current 30% (or below) of Imax ?
If I have an Inductor with high current rating, can the ripple current be 50% of Imax.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In general, the inductor ripple current can be any percentage you want. Originally, the percentage was set at 20-30% as it was assumed the minimum load current would be 10-15 % of full load and sizing the inductor that way will allow the converter to operate in CCM mode only (most early converters were non-synchronous). Also, for high ESR output capacitors, ripple voltage is directly related to inductor ripple current (VOp-p = ILp-p * ESR). Now with synchronous converters and low ESR ceramic output capacitors, that my not be a limitation. There may be limits based on your IC. Some have low side sinking current limit for example that could limit your p-p inductor current.
JohnTucker said:In general, the inductor ripple current can be any percentage you want. Originally, the percentage was set at 20-30% as it was assumed the minimum load current would be 10-15 % of full load and sizing the inductor that way will allow the converter to operate in CCM mode only (most early converters were non-synchronous). Also, for high ESR output capacitors, ripple voltage is directly related to inductor ripple current (VOp-p = ILp-p * ESR). Now with synchronous converters and low ESR ceramic output capacitors, that my not be a limitation. There may be limits based on your IC. Some have low side sinking current limit for example that could limit your p-p inductor current.
One more question -
How will sizing the inductor all the converter to operate in CCM mode only ?
If the p-p inductor current is less than twice the minimum load current, then the inductor current is always positive. DCM is enetered when inductor current falls to zero for non synchronous converters.