I'm using LP38501-ADJ to supply my GSM modem.. It's output is adjustable from 0.6V to 5V. I'm supplying it with 5.1V input. The formula given for calculation of output voltage is
I kept R2=10K ohm, V adj = 0.605v, I adj=750nA, required Vout = 4V so i got R1 = 56K ohm.. Is this correct?
But when i connected as per the above mentioned resistors, i'm getting no change in Vout. It's same as input Vin=5.1v. and V adj = 3.5V. It's not 0.605V.
1) What should i substitute for V adj and I adj?
2) What value of resistors (R1 and R2) should i use to get Vout = 4v?
Please help...