I am hoping someone can clarify equation 11 on page 13 of the datasheet of the TPS5420. The design example calculates a ripple current of 143 mA but i am unable to calculate the same value. As far i can tell the equation is:
Icout(RMS) = 1/sqrt(12)*[ ( Vout * (Vin(max) - Vout) ) / (Vin(max)*Lout - Fsw*0.8*Nc)]
where
Vout = 5 V
Vin(max)=36 V
Lout = 33 uH
Fsw - 500 Khz
Nc = 1
Plugging in the aforementioned equation in the above equations produces a Icout(rms) of -.112 mA NOT 114 mA.
So my question is: Is the equation i am using correct, if yes why do the values not line up, and if no where am i going wrong?
Thanks