Hello !
I am evaluating BQ34Z100EVM board with LiFeYPO4 12V 60Ah battery.
What value should I set for Design Energy after setting X10 bit to 1 and entering Design Energy Scale = 10?
The battery is LiFeYPO4 12V 60AH http://www.ev-power.eu/LiFeYPO4-batteries-12V-1-1/Lithium-Battery-12V-60Ah-WB-LP12V60AH.html?cur=1
Actualy it is 4 cell battery (3.2V each cell, Chem ID 0421) Are my calculation right?
(60000 mAh) x (3.2 V) x (4 cells) = 768000 mWh = 76800 cWh
Anyway value 76800 is out of range and couldn't be written into Design Energy data flash!
Thanks in advance,
Ilja