This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196 current limiting problem.

Other Parts Discussed in Thread: BQ24196

Hi!

I have current limiting problem with bq24196. Can anybody please tell me about the capicator b/w SW and BOOT is of 47nF or 47uF? In datasheet they have mentioned 47nf with 2.2uH. which exceeds the limit of LC filter frequency given in datasheet i.e(15KHZ-25KHZ).

I also setted the first 3 bits of Input Source Control Register REG00 to 111 in order to gain 3A of current but still the Input current doesnt exceed 500mA.

I will be thankfull if somebody can help me.