This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

power converter with accurate ADC and need to have std IO such as Ethernet

Other Parts Discussed in Thread: TMS320F2808

 

We have TMS320F2808 now controlling a power converter. Need much improved system: Some considerations

-there were some  issues with ADC.. SO added  key current mode/PID control in analog. The duty cycle correcting value  is fed to the ADC while before they were doing the c/m  through coding. Got very slow & problematic.

- perhaps should go for floating point dsp

- there is a need for providing all monitoring functions of converter to a host ......such  as Enable/disable, temp, load current, OV/UV, etc...Preferred method will be through Ethernet. Also prefer a "std IO code pkg"  that we can just use from a "library"

- implement the SYS/BIOS

Also: will model system and all other  Real Time code using matlab/RTW and use that code in CCS

 

which dsp will be most suitable to get all these done?

thnx

-robin