This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

supply for op-amps -- c. +/-15v ???

Other Parts Discussed in Thread: OPA2312, TPS65130, TPS65131

I have a system with the pcm179x (8 or 4a) DAC chip, with the op-amp output stage as shown in the datasheet (considering using 3x opa2312). This will lead to a power-amp which uses up to almost 3A at 13.5-14.5V. The DAC chip uses 5V and 3.3V which I can get pretty easily, but the op-amps require a +/- voltage up to +/-15V (best performance).

How would you recommend tackling this? I could use an AC-DC supply at 13.5-14.5V, and use this directly for the power amp, and the positive rail of the op-amps? If so what chip could i use to invert the voltage (-13.5:-14.5)? Or would using say a 24V supply be required, and regulating both the + and - ??. Simply, what is the most sane (cost-effective) way of fulfilling my needs?

  • Hello M.B.

    As far as I understand you, you have 3.3V or 5V available, but need +/-15V for OpAmps. You do not mention the average current you need on these supplies, but I would recommend checking out TPS65130 or TPS65131 (when more current is needed).

    Best regards,
    Brigitte