This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1901 Temperature Compensation

Other Parts Discussed in Thread: UC1901

Hello,

I am using the UC1901 Isolated Feedback Generator as a simple isolation amplifier similar to that shown in DN-19.  My circuit is slightly different from the design note in that I bias the NI pin with a fixed voltage less than the 1.5V reference (using a voltage divider).  The circuit is attached for reference.

I am able to get fairly linear response as long as the temperature of the UC1901 is somewhat stable (within a few degrees).  While precision is not super critical for this application I would like to compensate for the fairly large UC1901 output voltage swing as a function of temperature since my application requires -20degC to 60degC.  Does anyone have a suggestion for providing some temperature compensation for the UC1901 used as an isolation amplifier?  Thermistors for the voltage divider feeding the INV pin or elsewhere?  Thanks,

Bill