Hi! Is the SVID protocol of TPS51650 compatible to standard PMBus? I just need to set output voltage through SVID, without another functions. Also, may I use simple I2C bus for it?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi! Is the SVID protocol of TPS51650 compatible to standard PMBus? I just need to set output voltage through SVID, without another functions. Also, may I use simple I2C bus for it?
Thanks!
I am not 100% certain, but I think it is not directly PMBus or I2C compatible. If you are using the TI EVM, you can use the GUI software interface to set the parameters from a windows PC.
Hi Dimitry,
Please contact Rama Venkatraman directly. He is a system engineer for this part. His email address: rama-venkat@ti.com
Thanks,
Nancy