Hi, i want to use a DCP021212U IC (SO-28 Package) as an Isolated Voltage Source for a HighSide-Fet application.
Im currently testing the Device and there is a problem:
The input Voltage is 12VDC but the Output Voltage on the output side is about 24V and should be 12V ,too.
I also checked the Device Description, its actually a DCP021212U (not DU or something elese).
The input Capacitor is 2.2uF and the output capacity is 0.33uF. Both Ceramic , placed close to the IC.
Is it possible, that the device is damaged somehow? I cant find any solutions in the datasheet.
Thanks for your support