Dear LED Drivers Forum,
If I size the inductance properly for a minimum average current of 250 mA, can I expect any problems beyond a widening of the tolerance of that current? If I want to use the LM3414 for an average LED current of 250 mA, would it be better to operate it at 350 mA or 500 mA and then dim with a PWM signal? I´d prefer not to add the PWM circuitry if I could avoid it.
Thanks,
Chris