This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using the Command Line Tools in Fusion Digital Designer

Other Parts Discussed in Thread: UCD9222

Hi,

 I am wishing to use the command line tools available with the Fusion Digital Designer software as part of a automated production system to import a project onto a UCD9222.

  On a PC with the full Toolset installed I can successfully do this and all is well. However I wish to set this up now on  PC's in a production area and would like to avoid installing on each PC the full Fusion software package.  

I would be grateful, if somebody could point me to any documentation, that would allow me to do a minimal install solution on my production PC's. Is there for example a simple driver for the TI USB to GPIO card and a minimum set of dll's I need to run the command line executables  FusionDeviceExporter.exe and   FusionConfigWriter.exe

many thanks

Danny Thomson