This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5018 and LM5008A

Other Parts Discussed in Thread: LM5018, LM5008A, LM50, LM5008

Hello, 

I am trying to use a high input voltage converter ( up to 65V)  for a 3.3V at 200mA. I am currently using LM5008A which has the ripple config options. i am still getting about 30mV ripple on the Eval. Board. Do you have any ripple values on the LM5018. Webench gives about 2 to 3 mV andi just want to confirm with an apps engineer. My requirement is lower than 20mV. 

I am open to recommendations.

Regards,

Ismail