Hi:
I have a problem about TPS65070: My product need push down to ground always for PB_IN pin when the product is used.But the PGOOD will send a low pluse signal to reset CPU after the system is powered on about 15s.
I found that the PGOOD will be low after the PB_IN is kept 15s in the datasheet and descript that this is optional.So i think this function isn't fixed for TPS65070.I think the TPS65070 has different version. Isn't it ? And I have tested the TPS65070EVM board supplied by TI,this problem will not current,that is to say,the PGOOD hasn't low signal after the PB_IN pin is pushed low above 15s.And i have modified the TPS65070EVM board circuit same to my product circuit,the EVM board has not the low signal for PGOOD pin. So i think the TPS65070 has the different version chip, has not it? thanks!