Dear Non-Iso DCDC Forum,
I´m writing an article about using the TPS54160 with 1:1 coupled inductors, and for the control loop, I´d like to model the power stage more accurately than the basic transconductance gain given in the datasheet. The model I´d like to fit the TPS54160 to is the one developed by Robert Sheehan in his paper:
http://www.ti.com/lit/an/snva555/snva555.pdf
The information I need is the current sense resistance, the current sense gain, and the amplitude of the slope compensation ramp in V/us. (Or, if the slope compensation is variable, an equation to help me select it based upon a given set of operating conditions.)
Typical/average/most likely values are fine. Hopefully the development team of SwitcherPro has this information and could provide it.
Many thanks,
Chris