Hello I am very new the the bq27510 fual gauge and having a hard time finding the right info to write into the bqeasy battery info page.
Basically my questions are:
- On my datasheet for my battery it states that the nominal voltage is 3.7V (Average Voltage at 0.2C discharge) and on the same datasheet it also states that the cell voltage can be between 3.7 and 3.9V. Now after charging the battery the voltage sits at around 3.9-4 volts. Should I change the nominal voltage to 3.9V from 3,7V in bqeasy.
- What would be the best setting for the discharge cut-off voltage in bqeasy, the battery datasheet states that it is at 2.75V should i set it to 2.95V to be on the safe side when running the battery chemistry test.
These are probably very easy questions to answer so I hope someone can help me in record breaking time ;).