This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25088 Constant Current Question

Other Parts Discussed in Thread: LM25088

I'm an currently using the LM25088 to generate a 24V output from a 32V input. I want to add a feature of making sure the current will stay constant once the load reaches 10A. I was planning on using a simple transistor circuit to do this but I want to know if this chip already has this feature. I couldn't find anywhere in the data sheet that explicitly said that it would limit the current while remaining on. If anyone could tell me more about this it would be appreciated. 

Thanks in advance.