Hi,
at the moment I'm designing a circuit with the LDO TPS76150. In the datasheet (Version SLVS178B) is written that this regulator has a "Peak output current/current limit" of 100mA to 135mA. Does anyone know what that exactly means? I thought that this is the maximum output current e.g. if the output is shorted. But a measurement in the real circuit shows that the maximum output current is 163mA (see attached measurement results).
Did someone already make the same experience?
Regards