Sir:
I measure the REFIN pin is 0.9V after the voltage divider, but the output of VO and REFOUT are both 1.080V, and the PGOOD is in a HIGH state. Besides, I supply VLDOIN with 1.8V, and VIN with 3.3V and I confirm that these voltages are all right.
What is the possible problem for the VO and REFOUT output error?
Is there any debuggin procedure I should do to find the problem of the board?
Thanks
Jacky
2013-03-26