This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS84610EVM-003 / can be supplied 6A output current by EVM ?

Guru 20090 points
Other Parts Discussed in Thread: TPS84610
Hello,
 
In User's guide of TPS84610EVM-003, there is 4A rated output current in P.2 and there is 0.8V to 3.3V @ 4A in P.6.
Can be supplied 6A output current by this EVM ?
 
Since TPS84610 is integrated inductor and can output 6A current , so I think that I can use this EVM by 6A without problem.
But could you please kindly give me the confirmation?
 
Best Regards,
Ryuji Asaka.