Hello,
I have a custom circuit board which includes a bq24610 to charge a 2-cell Li-Ion battery from at 12V source. The circuit is taken from the datasheet with the following customizations.
ISET1 = 0.430V (Fast Charge Current = 2.75A)
ISET2 = 0.300V (Precharge Current = 1.18A)
ACSET = 0.808V (AC Current = 4.26A)
Vbatt = 8.42V (301K and 100K resistive divider to VFB)
Inductor = 6.8uH
When I power the AC Adapter with a 12V supply and connect a battery simulator, set for 7V with 0.030 ESR the stat lines show charging and REGN measures 6V. The LODRV is low duty cycle and the HIDRV doesn't go above 12V and then settles to the battery voltage. No net current flows into or out of the battery. I wonder if the internal charge pump isn't working properly to generate sufficient HIDRV voltage.
I have the bq24610evm board, customized as described above and it works with the same test setup. I noticed that the EVM board includes a 10-ohm series resistor on BTST which the datasheet doesn't have.
Attached are the HIDRV and LODRV waveforms.
Thanks,
-Ross