This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about QEN BQ34Z100 after learning.. ?

Other Parts Discussed in Thread: BQ34Z100

Hi Tom


1) to be presented at the end of learning learning Update Status
   Has been changed to 0x06.
 2) * gg file has been stored in the Note Book PC.

3) * gg files copied to mass-produced products to be recalled and Write after
    0x41? Please

4) Or do I need to change after Update Status 0x02 Reset 0x41?

3) Came by running the Reset 0x41 QEN Red from Green color
  Has been changed. Are you sure we're doing the right ..
4) shipment program for HDQ only do I need to Write?
     Or I2C .. possible?

for mass production products bq34z100 bulk use software program is downloaded and
Crime soge Please use ?

And BMS 16cell Supported by IC, a new stage. ?


Answer favor Dream.

 Shin

  • Shin

    It sounds like you have completed the learning cycle and Update Status = 06. You can follow the guidelines in SLUA334B to update the gg file and create the golden file. The production flow is discussed in several documents. It can be found in the Quick Start Guide. SLUA421A

    I attached the senc file that you will need.

    Regards
    Tom

    bq34z100_V0_06.senc