This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78PL114S12 - Max Error on SBData dynamic tab

Hello,

We noticed 'Max Error' on the 'SBData dynamic' tab. This value changes while using the battery. In the manual there is no information about this function.

How is this value calculated and what is the function of it?

Thank you.

  • Wim,

    At start of the device or after an initialization command, the value is 10. It is set to 1 when capacity
    learning takes place. The value increases by 1/20 for each cycle that goes by without learning. If it ever
    gets > 100, the CONDITION_FLAG bit of BatteryMode() is set.

    Regards
    Tom