This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3642 / Slave address, Mode change

Guru 20090 points
Other Parts Discussed in Thread: LM3642, LM3262
Hello,
 
I have some questions about LM3642.
Please kindly let me know about following.
 
----
(1) Slave address
Our custoemr use two of the LM3642 as slave by one of the I2C bus.
And LM3642 has one address(1100011) only. so customer can't use two LM3642 by one I2C bus.
Can I use LM3642 by other slave address or are there other slave address device ?
 
(2)Mode change.
We can change mode by Enable Register or device pins  "STROBE  pin " and "TX/TORCH pin" to High.
Which method of mode change has priority ?
 
(3)Processing of STROBE pin and TX/TORCH pin
If we control mode by I2C  , should we process STROBE pin and TX/TORCH pin ?
 
Since these pins are active high, should we tied GND?
Or , these pins  have internal pulldown , so can we float these pins ? 
 
Best Regards,
Ryuji Asaka