Are there any updates or work arounds to get the bq78PL116 API and USB-TO-GPIO module to work with Windows 7 64BIT? I notice some posts from TI employees which state there are no updated drivers for the USB-TO-GPIO for Windows 7. However, the bqWizard 3 software works fine on my Windows 7 x64 system while communicatiing with the bq78PL116. What is the difference between the API and bqWizard? What could be going wrong. They are both using the same USB-TO-GPIO driver, are they not?
Any input would be appreciated, thanks.