We are making a board with AM3359 and DDR3, and using the TMDSSK3358 Ref. Des. for guide with DDR3 connection and general power supplying.
The documentation about TPS65910 is very "dry". No intended method of use, minimal exemplification. (It could be developed a lot).
Our doubts:
Our board will be powered by a 5V Vmain, that we are using in place of VBAT (following TMDSSK3358 diagram), and we are intending to use VAUX33 to supply VDDIO. We infer that VDDIO is essential to mantain the control funtions alive (including sequencing), but, as we can see in the figure 3 of SWCU093B, VAUX33 is off for a reasonable period of time.
1) Is this connection correct?
2) What power rail mantains the internal chip logic on until VAUX33 rises?
3) There is other source of information about TPS65910 intended uses?
Thank you,
Luis