Hello,
I was trying my BQ25504 EVM and everything seems to work like it is supposed. The battery start charging and stops when it is supposed. Once, when I was discharging the battery with a load and without VIN, I removed the load and the EVM didn't work correctly any-more. After that, every time I put voltage to VIN the VSTOR keep unchanged. It seems like the switch between VSTOR and VBAT is locked or isn't working well. Any idea of how unlock this state or if the chip is broken?
Thanks in advance for your help.