This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dcdc isolated in:10V-32V out:1.5V..4V constant current 8A

hi

i need to build a dc dc converter.

it must be isolated for in to out.

accept min. 10V-32V as Input

output must have a more or less consant current of 8A

voltage on output 1.5V..4V  

the quality of the output signal is not critical .. i just load a lithium battery with it.

a low price is for the design is more important

 

pls help me choosing the right design and parts

THANK YOU

    roland