This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22670,LM22677...

Other Parts Discussed in Thread: LM22677, LM22670

Hello Mr/Ms,

 I will use LM22670-adj in topology Buck and inverter together with LM22677 in buck topology (3x CI LM22670 as buck, two CI LM22670 inverter, and one LM22677 as buck). I want to use the pin sync in all CI and I want to know if that is possible and how contect it. or only I have to attach the pin sync of all integrated circuits and one resistor to 1K to gnd like figure 4 (self synchronizing setup) of LM22670.

Thank you and best regards Jorge