Hello,
1) I just wanted to double check something with TI designers of LM4140. Looking at the datasheet for the LM4140 reference IC, it seems that the output impedance vs frequency graph (figure 8) starts from a negative value. If you zoom in, the thick line is clearly below the 0 (ohm) on the y-axis. Is this a typo or does the reference behave like a negative resistance in the range 0-3kHz??
2) If another AC source is attempting to drive the output of LM4140CCM-1.2/NOPB with a Thevenin impedance of 982kohms and voltage 500VACrms (60Hz), what is the resultant output due to the superposition of AC source and LM4140? I would expect that the LM4140 should just over-ride the AC source no problem, but I am seeing noise in the data which a 16-bit system easily picks up as 0.1mVrms. I haven't been able to measure the "superposition result" due to challenges in dealing with high-voltage probing, but needed some ideas about LM4140's behaviour. This should be explainable using the output resistance figure in the datasheet, which is where I am stuck at.
Thanks
Rahul