This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62170 inductance

Other Parts Discussed in Thread: TPS62170

Hi,

   I find 2.2uH inductance is used in TPS62170 for many different Vout, 1.0V/ 1.2V / 1.5V/ 1.8V / 2.5V / 3.3V /5V and -5V.

   1. Why is 2.2uH designed? The inductor current is differernt, doesn't it impact loop stability?  

   2. Is there any reason to use 2.2uH on all Vout?

 Alan