I have a board where I am using two LM22673 Simple Switchers. One is configured as a non-inverting regulator generating +12V at 1.4A and the other is configured as an inverting regulator generating -12V at 800mA. Both are fed from same +15VDC 4A regulated power supply. I used the Web Bench application to help design the circuit.
The prototypes worked perfectly for us. We ran 300 units. and about 20% of them exhibit a very audible whistling when tested under a load. The whistling sounds exactly like a tea kettle. It is possible to hear this sound coming right off the board. When we use the PCB to power our device, the whistling sound is coupled into the signal path, so it is a problem.
My guess is that this whistling sound is a beat frequency of the two switching frequencies. Since there is a tolerance of 10% in the switching frequency on the LM22673 (I think, I cannot remember exactly), perhaps there is some combinations of two switching frequencies that results in a beat frequency that is in the audible range.
Any help will be greatly appreciated.
Tony