This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9240 droop compensation

Other Parts Discussed in Thread: UCD9240

Is it possible to compensate for delivery droop with the UCD9240?

There is a known amount of resistance (8mOhm) between my measurement point, and the load. The supply is 1V, and the amount supplied is between 1A and 20A, so the droop is causing errors of more than 10%.