Hi,
We have designed the circuit which has BQ27510 for Li-ion Battery Monitoring.
The problem is if we didn't connect the external thermistor we are not able to read the Battery parameters like state of charge, remaining capacity etc.
The TS input is left open in the circuit
If we didn't connect the external thermistor only the Battery voltage is correctly read by the chip.
In the data sheet it is mentioned that we can use the on chip temperature sensor.
So i cleared the operation config flash register, Temps bit . This also didn't work around.
Is there any other settings to be done ?
Please guide us.