When working with the BQ25504 eval board and after having changed parameters of the BQ25504 to satisfy the application (charging Li battery), we remark that the input current of the card is always fixed at 110mA.
We do not really understand why this is happening.
Is there any way to get more energy out of it, knowing that solar panels are capable of delivering more than 300mA