This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650250 efficiency of LDO's

Other Parts Discussed in Thread: TPS650250

I can't find anywhere, the efficiency of the LDO converters. My board design is sensitive to even 1mA of wasted current.  I have implemented the circuit given below,  not using TPS650250 LDO's  because I cannot quantify their efficiency. I could save BOM, board space etc. if I knew the LDO's of the 650250 would be close to the 60% I get with the TPS73101.

I have all 3 of the switching regulators in use, so i cannot use one of them.

thanks

I have implemented a TPS73101 with 1.8V in and 1.2V out, at 10mA max, Webbench says it is 60% efficient at 8mA.   So my