I am currently trying to integrate several power supplies for use on a single PCB and one of them has me concerned. For all of the individual designs TI's webench was used as a starting point. One of the supplies will take 5 volts and produce -3.3V. Webench gave us an inverting buck boost topology using LM5088. We ordered an eval board for the LM5088, and modified it to match our Webench schematic. The circuit works as far as output voltage and current requirements. The concern I have is that on the particular circuit, for -3.3V output, we have to swap our gnd and vout. This poses a problem in that all of the supplies on the board will need a common gnd. Is there any way to integrate this circuit with the others (that I am missing), or do I need a different topology all together for this supply?
Device:LM5088MH-1/NOPB
Topology: Inverting_Buck_Boost
Design: 3601389/17 LM5088MH-1/NOPB