This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G3: Reading Wrong SOC values

Hi,

We are using BQ27520-G3 on one of the boards. We have an application which logs the battery charging current, SOC, Battery voltage etc. Please see the logs attached. The Fuel gauge is calibrated with help of TI support. We are seeing the SOC values read does not seem to be correct. The SOC is 0 even if the battery voltage reaches near to 4V and then starts counting. Finally when the charge termination current is reached, the SOC jumps from 79 to 100 directly. Can anyone help me how to correct this?

2656.OSCoreSVCTester.xlsx