This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AN-2241- SM72445 Eval Board

Other Parts Discussed in Thread: SM72445

Before explaning my doubt, thanks a lot to everybody in this forum.

I need to test some SM72445 Evaluation Boards (AN-2241) with SunPower 315Wp photovoltaic panels. Those panels have two caracteristics which mismatch with SM72445 Evaluation Board operating ranges:

- Vmpp 54,7V

- Voc 64,6V

______________________________________________________________

AN-2241 operating ranges:

-Vmpp: 15-40V

-Voc: up to 50V

I have to test 8 SM72445 Evaluation Boards using SunPower 315 photovoltaic panels so I would like to know please if this board could work with these panels changing their in and out capacitors to C3225X7S2A335M200AB (the same capacitor serie with 100V rated voltage), and their MOSFETS to IRFP4668 (VDSS = 200V, other parameters are similar).