We plan to use TPS24720 in our design.
I have few query.
- Can we use the IMON pin to monitor the current flowing through the device all the time.
- If yes then,
- Can we directly give the output to ADC
- What is the minimum current can it
- Which ADC TI recommends.
- If no then,
- Can we use figure 5 mentioned in http://www.ti.com/analog/docs/microsite.tsp?sectionId=560&tabId=2182µsiteId=7 accross Rsense of TPS24720. Will it disturb the current in Rsense resistor and hence disturb its performance and setting.
- If yes then,
- What does "Current Limit Function Enabled" means. On the TI page it is written that current limit function enabled is only during start-up.
- Does this means it will protect from in-rush only during start-up?
- Other functionality mentioned in the device are active only during start-up?