This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq3050 calibration with bqEVSW PC software

Other Parts Discussed in Thread: BQ3050, BQEVSW

Hi Ladies & Gents,

after calibration of bq3050 it is not possible to read the flash values from calibartion. It ends up with the message Runtime rerror '13', type mismatch. When verified this error message the bqEVSW software will shut down.
When I take the calibration parameters from screen and take them in the parameterfile.gg they are not written into the flash properly. E.g. the parameter CC gain should be in my case 0.27. As parameter it is written as 2700 in the parameter file, but the implemetation into flash will be 2700 and not 0.2700.

Is this a Windows problem based on German types?