This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding TPS65381-Q1

Dear, Sir.

TPS65381 includes Diagnostic and Watch-dog(WD) fuction. I would like to make sure the method to check all regulator output in an early phase of system develpment because MCU is not available yet.

1. At first, BATP and VBAT_SAFING with additional capaciors must be connected    to proper input voltage supply? 2. Is it needed to be disable WD fuction? 3. All regulator output check is avaliable under DIAGNOSTIC or ACTIVE modes? 4. Is there any special condition to check all regulator output?

Best Regards,