This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A10 as receiver coil

Other Parts Discussed in Thread: BQ51013, BQ500210

Hi,

I am trying to use off the shelf A10 coil (24uH)  as the receiver for a WPT solution. I am using bq51013 at the receiver side and bq500210 at the transmitter side.I use A10 coil at the transmitter side too. Every thing works fine until I react a load current of 600mA at which point voltage at RECT goes below 5.1V and the bq500210 shuts down. I want to go to 1A load current. I see that as the current increases( from 0 to 600mA) switching frequency increases. Is this normal? and since I do not have any control over the control strategy implemented in the transmitter side how do I go to 1A load with A10 coil.  

I also made a coil myself which has a lower self inductance (14uH) and it works fine. I can go to 1A load current. But not with A10 coil in the receiver. So I know that the circuit is not the problem.

What can I do to solve this problem?

Regards,

Sean

  • Hi,

     24uH inductor for the receiver is high, please use lower values to around ~10uH and make sure to tune the resonant caps as well in the receiver side.  

     Thanks

    Tahar

  • Dear Tahar,

    I have selected proper capacitors on the receiver side as per the WPC specification document. Moreover if you look at the document (http://www.ti.com/lit/an/slyt479/slyt479.pdf) which I used to design the receiver side, in table 1 on page 4, it is mentioned that a coil with dimensions 35X35 which has L22 of 22uH can be used to transfer 5W but I am only able to reach 3W (i.e., 5V and 0.6A). Could you please clarify? Is there a specific reason to use receiver coil lower than 10uH to reach a power transfer of 5W because this is something which is not very clear to me from the documents that I have read. 

    Thanks for the quick reply.

    Sean

  • Sean,

     Please work with the local TI sales office to provide you with design guidelines documents.

     Tahar