This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thought of using the TPS3808G125 as a single power on reset for a 3.3V circuit

hello there ,

i need to apply a single (one-shot) POR circuit at the power up of the card - however the costumer does not want the main voltage (3.3) to be monitored since he does'nt want any "active" reset in his card.

can i supply the TPS3808G125 with 3.3V (and i know it will reset when the voltage goes above or drops below the aprox. 1.16V).

will thank for any ideas

Dan