Technical Information!!! TPS65258 EVM
How can I setup the USB Switcher on the board? I mean ...can I feed the Vin of the USB switcher with the out of one of the Buck converters ? It will be enough the 3.3 V or I will need an external DC source of 5V? How can I enable the USB switcher with AN external drive signals?
Thanks...