I am planning to use this driver TLC5971, to handle strings of HB RGBW LED from Cree, Inc. RGBW means the 3 color plus Cool White in one single die, HB means high Bright LED, the typical forward current is 350 mA. The maximum current from the TLC5971 is 60 ma per channel. There is any suggestion on how to handle more current without loosing linear control if I need to add for example a MOSFET transistor? Or there is another TLC driver that can handle by itself those RGBW LEDs.?
Thank you for your reply.
Julio