Hello,
I just stumbled upon a detail that I previously missed. On the bq77PL900EVM reference design, VC11 is connected to the cell via a resistor, as with the other VCx (SLUU324, p.21). However, in the datasheet, it's absolute maximum rating is stated as -0.3 V .. +0.3 V with respect to GND. Wouldn't this likely be exceeded when the balancing fet is turned on (4,2V * 400 / (400+2*510) = 1,2 V) ?
We used the bq77PL900 in low volume designs with schematics very similar to the EVM (including the forementioned resistor at VC11, that is). There haven't been failures so far. Plus, the EVM will have been rather widely spread as well, and appears to work fine in our case. What am I missing in the calculation above? What is the motivation for the narrow range of VC11 maximum ratings?
Thanks in advance,
Joerg