This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

110~285VAC to 9VDC 2000mA LED power supply.

Hi,

Which driver IC should I use for my LED light? Following are the parameters of power input and output.

Input voltage 110~285VAC

single output 9VDC, 2000mA [2x3 LEDs of 1watt each]

Thanks.

Bhavesh. Nasik.